This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE CC2640 Stack 编译错误

Other Parts Discussed in Thread: CC2640, SYSBIOS

因学习项目需要,要在一个别人的项目上做些改动,但是stack怎么便宜都不行。不知道到哪里去下载这个“CC2640\Libraries\CC26xx\IAR\”。在下新手白丁一个,恳请各路大神帮助一把,在此拜谢了。

Building configuration: CC2640Stack - FlashROM
Updating build tree...

Performing Pre-Build Action
C:\Projects\tracker-firmware\IAR\Stack\CC2640\TOOLS\LibSearch\LibSearch.exe C:\Projects\tracker-firmware\IAR\Stack\CC2640\buildConfig.opt C:\Projects\tracker-firmware\IAR\Stack\CC2640\
TOOLS\LibSearch\params_split_cc2640.xml C:\Projects\tracker-firmware\IAR\Stack\CC2640\Libraries\CC26xx\IAR\ C:\Projects\tracker-firmware\IAR\Stack\CC2640\LIB\CC2640Stack.a FlashROM
<<< ERROR >>>
Cannot find input file "C:\Projects\tracker-firmware\IAR\Stack\CC2640\Libraries\CC26xx\IAR\"
<<< /ERROR >>>
Error while running C:\Projects\tracker-firmware\IAR\Stack\CC2640\TOOLS\LibSearch\LibSearch.exe C:\Projects\tracker-firmware\IAR\Stack\CC2640\buildConfig.opt C:\Projects\tracker-firmware\
IAR\Stack\CC2640\TOOLS\LibSearch\params_split_cc2640.xml C:\Projects\tracker-firmware\IAR\Stack\CC2640\Libraries\CC26xx\IAR\C:\Projects\tracker-firmware\IAR\Stack\CC2640\LIB\CC2640Stack.a FlashROM 


Total number of errors: 1
Total number of warnings: 0

  • SDK 要求对应的IAR版本以上吗? Stack不需要改动,默认指定IAR下编译都可以通过

    例程位置有改动吗?

  • 请提供你的IAR及SDK版本信息

  • IAR EWARM 8.10.1

    BLE SDK ble_sdk_2_02_01_18

    我想问下编译Application之前是否一定要先编译Stack?

    Stack具体是起什么作用的呢?

    怎么能在别人的project里找到它所用的所有library和SDK的版本号(如果问不到作者本人的话)?

    另外,Pre-build option中用了LibSearch.exe,它的参数中有“$PROJ_DIR$\Libraries\CC26xx\IAR\”。但是我在所有的文件夹中都找不到这个“Libraries”文件夹。

    (我是零基础小白。。。)

  • 这个版本符合要求了。零基础的话, 建议根据C:\ti\simplelink\ble_sdk_2_02_01_18\docs里的文档操作,尤其是SWRU393_CC2640_BLE_Software_Developer's_Guide

  • Hi Viki,

    现在的编译Application的build message如下:

    warning: xdc.cfg.Program: "C:/ti/tirtos_simplelink_2_13_01_09/products/bios_6_42_00_08/packages/ti/sysbios/hal/Hwi.xs", line 181: xdc.cfg.Program stack: For IAR targets, Program.stack is ignored. The C and Hwi stack sizes are determined by the size of the
    CSTACK section definition within the linker command file.
    generating custom ROM library makefile ...
    Starting build of library sources ...
    making C:/Workplace/tracker-firmware/IAR/Config/src/sysbios/sysbios.arm3 ...
    gmake[1]: Entering directory `C:/Workplace/tracker-firmware/IAR/Config/src/sysbios'
    Preprocessing library source files ...
    Creating the SYS/BIOS library that contains the APIs not included in the ROM ...
    __TA_xdc_runtime_Error_Data__arg arg;
    "C:/ti/xdctools_3_31_01_33_core/packages/xdc/runtime/Error.h",85 Error[Pe1061]:
    declaration of field "arg" is incompatible with a declaration in
    another translation unit
    field "xdc_IArg [2] arg" (declared at line 85) (from translation
    unit "mangled_ti.sysbios.BIOS_config_lib.pp")
    field "xdc_IArg [2] arg" (declared at line 85) (from translation
    unit "mangled__BIOS_lib.pp")
    detected during compilation of secondary translation unit
    "mangled_ti.sysbios.BIOS_config_lib.pp"
    xdc_runtime_Types_Site site;
    "C:/ti/xdctools_3_31_01_33_core/packages/xdc/runtime/Error.h",97 Error[Pe1061]:
    declaration of field "site" is incompatible with a declaration in
    another translation unit
    field "xdc_runtime_Types_Site site" (declared at line 97) (from
    translation unit "mangled_ti.sysbios.BIOS_config_lib.pp")
    field "xdc_runtime_Types_Site site" (declared at line 97) (from
    translation unit "mangled__BIOS_lib.pp")
    detected during compilation of secondary translation unit
    "mangled_ti.sysbios.BIOS_config_lib.pp"xdc_runtime_Types_Label *(*__label)(xdc_Ptr, xdc_runtime_Types_Label*);

    然后是一堆类似的error,最后说:

    Fatal error[Ms016]: Error limit reached
    Fatal error detected, aborting.
    gmake[1]: *** [mangled__BIOS_lib.obj] Error 2
    gmake: *** [C:/Workplace/tracker-firmware/IAR/Config/src/sysbios/sysbios.arm3] Error 2
    error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/SourceDir.xs", line 209: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2:
    js: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
    xdctools_3_31_01_33_core\gmake.exe: *** [package/cfg/appBLE_prm3.xdl] Error 1
    xdctools_3_31_01_33_core\gmake.exe: *** Deleting file `package/cfg/appBLE_prm3.xdl'
    xdctools_3_31_01_33_core\gmake.exe: *** [package/cfg/appBLE_prm3.xdl] Deleting file `package/cfg/appBLE_prm3.h'
    xdctools_3_31_01_33_core\gmake.exe: *** [package/cfg/appBLE_prm3.xdl] Deleting file `package/cfg/appBLE_prm3.c'
    js: "C:/ti/tirtos_simplelink_2_13_01_09/products/bios_6_42_00_08/packages/iar/tools/configuro/Main.xs", line 93: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
    Error while running "C:\ti\xdctools_3_31_01_33_core/xs" --xdcpath="C:\ti\tirtos_simplelink_2_13_01_09\products\bios_6_42_00_08\packages" iar.tools.configuro -c "C:\EWARM\arm" --cc "C:\EWARM\arm\bin\iccarm.exe" --device "CC2640F128" --compileOptions

  • 在工程的目录里有个configPkg文件夹,下有error.log,对照下看看是什么错误

    个人觉得还是编译器或者系统的问题,建议重装一下或者换台电脑试试,而且软件及TI例程建议都安装在默认路径,不要改动