TI E2E™ 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SmartRF Studio version 2.19.0 导出的参数无法正常使用

Other Parts Discussed in Thread: CC1352P

专家你好

       开发板是cc1352P2,工程是C:\ti\simplelink_audio_plugin_3_30_00_06\examples\rtos\CC1352P_2_LAUNCHXL\easylink\rfAudioTx、Rx。我在SmartRF Studio version 2.19.0中选择(500 kbps, 2-GFSK, H=0.76, IEEE 802.15.4g MR-FSK PHY mode),并将配置导出为c文件,替换smartrf_setting.c和.h,但是发现TX能正常闪绿灯,RX则不能闪灯。使用(200 kbps, 2-GFSK, 100 kHz deviation, 868 MHz)遇到同样的问题。500kbps与200kbps的变量都是rfc_CMD_PROP_TX_ADV_t RF_cmdPropTxAdv或rfc_CMD_PROP_RX_ADV_t RF_cmdPropRxAdv。

      如果用(1 Mbps, 2-GFSK, 350 kHz deviation (868 MHz)),则正常收发,且其变量为rfc_CMD_PROP_RX_t RF_cmdPropRx或rfc_CMD_PROP_TX_t RF_cmdPropTx。

      SmartRF Studio version 2.18.0中200kbps可以收发正常,但是SmartRF Studio version 2.18.0没有500kbps。

      请问专家,我们怎么在SmartRF Studio version 2.19.0 版本中导出能使用的RF配置文件,要做何修改?