This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: 关于AOA角度算法以及天线的相关问题

Other Parts Discussed in Thread: SYSCONFIG

您好,

1、给的例程,这+-5度的波动主要是什么引起的呢?这个波动的角度数值,有什么分布规律吗?(例如正态分布...?)

2、我在空旷的环境下,进行测试,在下面的图里,1是mater 2是passive加AOA天线板,在图中标示0°线的有半面测量出来的数据都是在40度大跨度的波动,左半面只有在距离0°线45°以内的数据较为稳定,能在10°波动,超过45°,就数据也不行。 和所说的可以在120°范围测量怎么出入这么大呢?   这是什么原因导致的呢?(我的测量都是在slave距离passive1米测得,测试场地也是在没有wifi信号、在粗糙的地上进行的,距离墙面有1.5米的距离。)