This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541: CC2541加PA只使用TX和RX

Part Number: CC2541
Other Parts Discussed in Thread: CC2590

有关CC2541加PA的程序设计方面有以下几个疑问(协议栈版本1.3.2)

1、协议栈中HCI_EXT_ExtendRangeCmd这个HCI指令默认是对P1_1、 P1_2、 P1_3这3个引脚都进行了设置吗?由于我们的硬件设计上只是将P1_2和P1_3用于PA  

P1_1引脚用于按键,所以会设置成上拉输入以此来检测下降沿 。所以想问一下如果只用P1_2、P1_3这两个引脚射频用应该怎样配置相应的寄存器。

2、命令行中的HAL_PA_LNA_CC2590这个宏如果不使能的话会不会对PA的设置有影响(只用P1_2、P1_3这两个脚)。

3、对于进入低功耗时如果没有执行HCI_EXT_ExtendRangeCmd这个指令及禁止HAL_PA_LNA_CC2590这个宏的前提条件下是否需要将P1_2、P1_3设置成普通IO并且设置成低电平使PA芯片处于低功耗状态。如果将P1_2、

P1_3这两个引脚由射频观察映射脚设置成普通IO需要进行哪些特殊的寄存器配置。