由于国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101和CC1310 哪个功耗低。

Other Parts Discussed in Thread: CC1101, CC1310, TPS62730

CC1101和CC1310 哪个功耗低。睡眠和发送状态下。

  • CC1310发送功耗低,CC1101只是transciver,沒辦法跟CC1310直接比較睡眠状态

  • 功耗数据可以查看各自的数据手册
    CC1310: 宽电源电压范围:1.8 至 3.8V
    RX:5.4mA
    TX(+10dBm 时):13.4mA

    CC1101:In RX, the current drawn from a 3.6 V battery is typically less than
    11 mA when TPS62730 output voltage is 2.1 V. When connecting CC1101
    directly to a 3.6 V battery the current drawn is typically 17 mA
    In TX, at maximum output power (+12 dBm), the current drawn from a
    3.6 V battery is typically 22 mA when TPS62730 output voltage is 2.1 V.