This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310 电源管理用户操作问题

Other Parts Discussed in Thread: CC1310, CC2640R2F, CC2630, CC3200

咱们的1310有个电源管理文档,里面有不少API,我想知道这个是不是被RTOS融入进去了,用户不用操心这方面的功耗优化问题?

  • 你说的是这个---CC26x0, CC13x0 SimpleLink™ Wireless MCU Power Management Software Development Reference Guide?是基于TI RTOS的
    Power management for the CC26x0 and CC13x0 SimpleLink ultra-low-power wireless MCU platforms is implemented as part of the TI-RTOS kernel.
  • yes,回头看了一下,在IAR开发环境中有两种安装,一个是simplelink 一个是TI-RTOS 这两个有什么区别吗?
  • TI-RTOS 捆绑在SimpleLink SDK中的
  • 任意使用它们之一都可以是吧
  • TI RTOS有自己的SDK,simplelink下的芯片也有各自的SDK,对于CC1310来说,SDK是基于TI RTOS的,直接用SimpleLink SDK就行了

    To obtain TI-RTOS for Microcontrollers (MCUs)

    To use TI-RTOS with TI's SimpleLink™ SDKs – Click the appropriate “Get Software” button above. Note that for more recent TI devices, including the CC3220, CC2640R2F, and CC13x0, TI-RTOS support is only available as part of the SimpleLink SDK.

    To use TI-RTOS with other TI MCUs and Wireless MCUs – Click the TI-RTOS “Get Software” button above. Device families supported include the ARM® Cortex™-M4 Tiva-C, C2000™ and MSP430™ microcontrollers, as well as the SimpleLink™ WiFi® CC3200 and SimpleLink™ CC2630/40/50 ULP Wireless MCUs.

    To use TI-RTOS with Code Composer Studio IDE Desktop – Download and install the latest CCS version. Once installation is complete, run CCS and download the appropriate SimpleLink™ SDK or TI-RTOS release through the CCS Applications Center.

    To use TI-RTOS with Code Composer Studio IDE Cloud – Go to dev.ti.com

    To use TI-RTOS with IAR Embedded Workbench or GCC – Click “Get Software” button above and download the latest TI-RTOS version. See release notes for compatible tools versions.