目前想用CC2640的电容按键来实现上下滑动以及确认功能,类似于笔记本的触摸功能。如果实现该功能的话,需要几个按键?原理以及PCB的pad该如何设计?请帮忙回答一下。急需。非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢你的回信。但我还是有两个问题需要确认一下:
1、请问CC2640是否支持CAP touch功能?因为你给的是CC26X2的,而且对于CC13X2也不太需要吧?CC2640内部不是集成了蓝牙模块吗?
2、我只需要CAP touch功能,看里面的设计cap touch 三个信号与连接插件直连,这三个信号该如何与CC2640连接?
为什么选择CC2640,主要是考虑他集成了蓝牙模组的同时,而且有个较小的尺寸可以选择。目前对尺寸要求比较严格,所以选择的是CC2640R2FRHB(5mmX5mm)。这也是为什么反复要确认CC2640本身是否支持?如果选了CC26X2,他的尺寸只有7mmX7mm,比较难满足要求。
嗯,不像430,CC2640本质上是用ADC实现的,就是要用支持模拟输入的口。
BR. AZ
SimpleLink CC2650 EVM Kit 4XS (CC2650EM-4XS) v1.0.4 Design Files
you can copy the single ended Front end design.
BR. AZ