1、我想将cc1310应用在718Mhz-878Mhz频段,是否无需关心芯片的A/B版本?,即所有CC1310芯片都可以适用于这个频段?
2、cc1312/1352是否也是可以用于718Mhz-878Mhz这个频段的?如果可以的话,一个音频应用产品(需要500kbps空中速率,私有协议,需要用到I2S+I2C+SPI接口,14dbm输出,使用板载天线)不考虑主CPU核性能和内存大小差异时,整个硬件设计特别是射频设计是否支持从CC1312到CC1310的无缝转换?
3、如果在量产产品中使用RSM封装的CC1310,需要用到I2C,I2S和SPI接口,请问是否DIO_0到DIO_9都是可以任意组合并分配给这些外部接口使用?比如DIO0-4用于I2S,DIO5-6用于I2C,7-9用于SPI?
4、如果以上都可行的话,是否可以先使用LAUNCHXL-CC1312R1+外接codec板的方式来快速评估(主要是评估718Mhz-878M频段,14dbm输出,500kbps下使用板载天线时的传输距离)?评估时有什么需要特别的注意事项吗?