LAUNCHXL-CC1350
sensor and collector example FH mode,
配對入網後 sensor 端的 UART 會一直都到 dataCnf: 64
請問這是什麼意思,哪裡可以查到狀態的意義?
感謝!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LAUNCHXL-CC1350
sensor and collector example FH mode,
配對入網後 sensor 端的 UART 會一直都到 dataCnf: 64
請問這是什麼意思,哪裡可以查到狀態的意義?
感謝!
macMcpsDataCnf_t dataCnf; /* MAC_MCPS_DATA_CNF */
/* MCPS data confirm type */ typedef struct { macEventHdr_t hdr; /* Contains the status of the data request operation */ uint8 msduHandle; /* Application-defined handle value associated with the data request */ macMcpsDataReq_t *pDataReq; /* Pointer to the data request buffer for this data confirm */ uint32 timestamp; /* The time, in backoffs, at which the frame was transmitted */ uint16 timestamp2; /* The time, in internal MAC timer units, at which the frame was transmitted */ uint8 retries; /* The number of retries required to transmit the data frame */ uint8 mpduLinkQuality; /* The link quality of the received ack frame */ uint8 correlation; /* The raw correlation value of the received ack frame */ int8 rssi; /* The RF power of the received ack frame in units dBm */ uint32 frameCntr; /* Frame counter value used (if any) for the transmitted frame */ } macMcpsDataCnf_t;
一般如果数据请求发送到其条目是不在邻居表中的节点,则会发生 dataCnf: 64 。