This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPSTK-CC1352R: XDS110出現 Error -267 @0X0 錯誤

Part Number: LPSTK-CC1352R

您好,執行到一半突然間出現以下錯誤

Error connecting to the target:
(Error -267 @ 0x0)
The controller could not detect valid target supply. Check target
JTAG connection and/or connection setting specifying voltage level.
(Emulation package 9.5.0.00143)

但是板子是有下載過程式的,而且先前燒錄的程式也是可以正常執行的

但只要接上XDS110進行編譯就會出現這項錯誤

換另一個板子卻又可以正常工作

請問這是甚麼原因呢?

  • 检查供电及连线是否正确:

    The error below happens if a XDS110 is being used, the Power Selection setting is set to Probe supplied power but the hardware itself is not properly providing power to the target device. In this case, verify if all power connections or launchpad jumpers are correctly connected.

    Error connecting to the target:
    (Error -267 @ 0x0)
    The controller could not detect valid target supply.
    Check target JTAG connection and/or connection setting specifying voltage level.

  • 您好,感謝您的回覆

    我好像已經解決這個問題了

    LPSTK-CC1352R 是用電池供電的

    我發現應該是電池的電壓用太久

    電壓不足所致,雖然板子可以正常工作

    但是電壓準位不夠,所以XDS110不能正常工作

  • 这是可能的,你更换新电池后试一下