This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

433M射频天线硬件设计

Other Parts Discussed in Thread: CC430F5137, CC430F5133, CC1101

目前项目在使用CC430F5133(与CC430F5137是一个系列),设计频率为433MHz,在天线设计上有些问题,想请教一下:

1、CC430F5133这款芯片,在没有外部射频功放的情况下,仅靠芯片自身可以达到多远的通信距离(在空旷场地上)?

2、关于天线的硬件设计,官方的参考如下图所示;但同时这款芯片的无线部分是一个CC1101,我查找了CC1101的天线参考设计,如下图所示;这两种设计孰优孰劣?个人认为:CC430F5133的天线设计为了兼容433、868和915的不同频率,而CC1101则特别说明了是315/433M频率的天线设计,是否有这方面的影响?因此CC1101的设计更适合我的应用?

3、在CC430F5133的参考设计中L6在433M的说明是dnp(do not populate),是否我在硬件设计时可以去掉这个电感?

4、天线部分在PCB设计中,电容电感的布局是否一定要和原理图一样,当然这可能是最好的效果,但要是由于PCB尺寸有限制,我在布局时进行弯折(例如在CC430F5133的天线设计中在C27这点弯折,其后的部分转90度,那么天线部分可以缩短一半的长度),不知道这样会对实际的信号传输有多大影响?

5、在PCB布局上,天线部分的周围是否最好不要放置其他的外设芯片(例如电源管理或者传感器等),可能会影响到天线的信号传输?

不好意思,由于小弟刚刚接触射频这方面,没有太多的经验,问题比较多,而且有些问题可能比较幼稚,还望各位不吝赐教,万分感谢!