This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问CC1100和CC1100E的区别?谢谢!

Other Parts Discussed in Thread: CC1100, CC1101, CC1100E

您好:

        我们最近在做的一个项目中,本身要用到CC1100,将其工作频点设置在915MHZ,

而在采购部门在采购器件时,误将CC1100采购成CC1101E,从cc1101e的数据手册来看,

cc1101e应该是不支持915MHZ的,而奇怪的是,它竟然和CC1100能够通讯,而且是正确的。

请问该现象该如何解释?谢谢!

  • CC1100E是支持470MHz  - 510 MHz, 950 MHz - 960 MHz 的。你需要915 MHz 应该采用 CC1101。CC1100 是一颗老的料,已经被 CC1101 替换了。强制使用一颗料在非推荐频段,射频性能没有保障。

  •         你好!我还有一个问题,我们还有一批cc1101的电路板,这次焊接了20块,只有一块可以和以前调试通过的板子正常通信,19块板子都不行。我们检查芯片射频管脚的直流电压都是在0.9V到1.0v之间,跟正常的板子一致,设置gdo0的测试管脚为时钟,也正常,读1101的状态,设置idle、tx、rx也都正常。我们现在怀疑1101底下那个焊盘的焊接问题。底下焊盘是按照手册的推荐layout做的,但是钢网文件却将该焊盘漏掉了,有可能造成底下焊盘接地不好。 因为拆焊比较麻烦,您能否帮我确认下,是否有可能是该问题造成的,谢谢!