请问WIFI模块WL1807MOD的功耗如何计算?电源VBAT接固定3.3V是否可以?手册中说VBAT上会有700多mA的瞬态大电流,在设计时针对此问题有啥要注意的地方吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问WIFI模块WL1807MOD的功耗如何计算?电源VBAT接固定3.3V是否可以?手册中说VBAT上会有700多mA的瞬态大电流,在设计时针对此问题有啥要注意的地方吗?谢谢!
Hai,
wifi链路是一个非同步系统,和上下行业务关系很大。没办法计算的。但一些特殊场景是可以标出的,比如idle connection啥的。
我咋没见到700多mA的标示,那一页呀?
BR. AZ
1)手册的第29页注释(2)显示:device calibration时VBAT上的峰值电流达到850mA,设计时需要有啥特殊考虑的地方吗?2)VBAT接固定的3.3V可以吗?3)计算WLAN发射时的最大功耗可以按照表格5.7.5中给出的WLAN current的最大值510mA计算吗?即最大发射功耗=VBAT*510mA,这样计算对吗?
hai,
1. 2,
谢谢看到了。那就按照note里面 The maximum VBAT value is based on peak calibration consumption with a 30% margin.
2)3.3V 可以的
3) 不行。原因就是wifi不是一直发,是收发分时的。和业务相关,无法计算。
BR.AZ