TPS54362-HT空载时输入侧有80mA左右电流(输入24V,输出12V),请问这个正常吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
理论上是不正常的,该器件的静态电流是65uA,考虑到其他损耗,空载应该不会超过这个值太多。建议查看我们的EVM的电路
https://www.ti.com/tool/cn/TPS54362BEVM
ILimit(防止过冲)为80mA,意味着在输出电压(VReg)低于设定的过压阈值(OV_TH)时,器件会限制输出电流至80mA,以防止过冲或损坏。
没太理解,输出电压(VReg)低于设定的过压阈值(OV_TH)时,器件会限制输出电流至80mA。OV_TH是过压门限,正常工作时通常都是不过压的,即0<OV_TH<0.8V,按这样说的话器件会一直限制输出电流至80mA?
在正常工作条件下,如果OV_TH没有触发过压保护,TPS54362-HT将根据负载需求提供电流,而不是一直限制在80 mA。只有在特定的故障条件下,器件才会限制输出电流以保护自身和负载。
当 OV_TH > 0.8V 时,表示过压保护功能被启用,否则关闭。
如有其他问题,请重新发布一个新帖。