使用Uniflash->Create Image,mcuimg.bin大小200KB,Service Pack File大小161KB,Capacity选择的1M时报错,而选择2M或者更大才正常,想问下如何能使选择1M容量时生成成功?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用Uniflash->Create Image,mcuimg.bin大小200KB,Service Pack File大小161KB,Capacity选择的1M时报错,而选择2M或者更大才正常,想问下如何能使选择1M容量时生成成功?
请问能否给出您设置的相关截图?另外您可以参考下E2E上的类似问题
https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/945030/cc3235sf-uniflash-error-when-flashing-to-a-cc3235sf-based-hardware
感谢回复,我试了一下使用Development 模式和Production模式效果是一样的。不过当我将Service Pack File去掉,并且将mcuimg.bin替换成105K时,1M BYTE的生成成功了,但是我将这个生成成功的 .sli 文件往我外挂1M flash的板子上烧录时提示烧录失败。
问题:
1. 如果我生成的Image中不包含Service Pack File会有什么问题?
2. CC3235S能否外挂 1M 的flash?
1. 如果我生成的Image中不包含Service Pack File会有什么问题?
参考之前链接内的说明
The service pack is a file that contains fixes and new features for the network processor code. At a minimum the service pack is required to be programmed, and you should always use the latest released service pack.
这个是需要包含Service Pack File的
2. CC3235S能否外挂 1M 的flash?
Unfortunately no, the CC32xx devices cannot support XIP from external flash.
e2e.ti.com/.../cc3235mods-add-an-external-1mbit-flash