Other Parts Discussed in Thread: CC1352P, CC2652P, SYSCONFIG
使用的例程是examples\rtos\CC1352P_2_LAUNCHXL\thread\cli_ftd,tirtos,gcc,IDE是CCS。
硬件平台是LAUNCHXL-CC1352P-2 Rev:B
测试流程,以下流程中LAUNCHXL-CC1352P-2板子简称1352:
1.烧录运行例程;
2.使用ifconfig up命令开启射频;
3.使用scan命令扫描router信息;
4.使用txpower 20设置发射功率;
5.使用scan命令扫面router信息 -- FAILED;
6.使用ifconfig down关闭射频;
7.使用txpower 15设置发射功率;
8.使用ifconfig up开启射频;
9.使用scan命令扫描router信息 -- FAILED;
10.使用ifconfig down关闭射频;
11.使用dataset命令生成网络参数并应用;
12.使用ifconfig up及thread start运行射频和thread协议栈;
13.等待成为leader;
14.使用CC2652P(自己设计,简称2652)作为节点,扫描router信息,可以获取到板子的信息;
15.通过txpower设置1352的发射功率,分别测试5,15,20dbm,2652都能扫面到板子信息;
16.关闭1352的射频及thread协议栈,设置发射功率为20dbm;
17.打开1352射频,使用scan扫描router信息 -- FAILED;
18.使用示波器测试PA最前端,靠近模拟开关处的电容位置,然后扫描router信息 -- OK;
19.用手触碰此处电容焊盘,然后使用scan扫描router信息 -- OK;
20.测试蓝牙例程的PA功能,一切正常。
上面流程中异常的步骤分别是5,9和17,希望能帮忙看看异常的原因可能是什么?