Other Parts Discussed in Thread: CC1352P, , CC2640, LPSTK-CC1352R
终端设备使用开发板上的3.3V电源供电上电可以正常入网,使用3.6V锂电池上电后无法正常入网。锂电池通过LDO稳压到3.3V后再供电给模组,则可以正常入网。请问是怎么回事?电路设计是参考1352P开发板画的。如图EF50模块为外挂LDO,可以正常入网,5D88模组无外挂LDO,无法正常入网。异常入网.zip正常入网.zip
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用电池供电参考:https://www.ti.com.cn/cn/lit/an/zhcaac1c/zhcaac1c.pdf
其他的我周一看一下回复你
你好,你这边提供的《 优化 SimpleLink CC1352P 以在 10dBm 输出功率下通过纽扣电池供电 》主要说的是电池电流低的情况下的应用,我现在测试使用的是可调电源,电流调到500mA以上,电压在3.8V时,能收到组网成功的Device annouce,后面就没有了。数据通讯无法正常进行。电压从3.8V慢慢往下调,当电压下降到约3.4V-3.5V的时候,通讯正常。再往上调的时候数据通讯又中断了。这好像与芯片规格书上的电压工作范围有矛盾
电池供电通常需要使用外部稳压器,它可以保证CC2652P和其余外设始终获得稳定的电源电压,而与电池电压无关,从而确保整个系统的稳定运行
我们有一个CC2640的使用外部稳压器的参考设计:https://www.ti.com/lit/an/swra498/swra498.pdf?ts=1635759813234
也可参考LPSTK-CC1352R的参考设计,它也是使用电池供电的:https://www.ti.com/tool/LPSTK-CC1352R
电压从3.8V慢慢往下调,当电压下降到约3.4V-3.5V的时候,通讯正常。再往上调的时候数据通讯又中断了。这好像与芯片规格书上的电压工作范围有矛
使用稳压电源测试,我相信在1.8V-3.8V范围内任一的稳定电压下都可以正常工作,如果动态调整,出现上述问题是有可能的,要注意控制供电电压的纹波