LaunchPadXL-28377S的接收跑can_ex5_simple_receive.c为什么只有接收的rxMsgCount在变化,但是接收数据是空的什么原因呢?麻烦帮忙测试一下!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LaunchPadXL-28377S的接收跑can_ex5_simple_receive.c为什么只有接收的rxMsgCount在变化,但是接收数据是空的什么原因呢?麻烦帮忙测试一下!
我会在下午使用28379D launchpad来测试一下
你好这个问题我自己已经搞定了。最后还要麻烦您一下,CANA是不是不支持扩展帧呢?
最后还要麻烦您一下,CANA是不是不支持扩展帧呢?
可以支持的
Extended frames can be stored only in message objects with Xtd = one, standard frames in message objects with Xtd = zero
你好这个问题我自己已经搞定了
很高兴您能解决问题
那麻烦问一下,CANA和CANB的区别呢?CANA支持CAN1.2,CANB支持CAN2.0?仅此而已么?
The CAN module implements the following features:
Complies with ISO11898-1 (Bosch® CAN protocol specification 2.0 A and B)