This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24612: 移相全桥芯片驱动提前关断

Part Number: UCC24612

如上图所示,系统拓扑为移相全桥电路,1通道为同步整流开关管漏源极电压波形,可以看到由于续流阶段电流下降,DS间电压逐渐下降接近0,进而导致UCC24612驱动关断,关断后开关管的体二极管继续导通,但UCC24612却无法再度给出驱动信号。请问:

1、此种情况为何会产生,DS间反向电压已经大于开通阈值了,为什么芯片无法开通。

2、此时负载较小,如果进一步增大电流,使得DS最小负向电流大于关断阈值,那么芯片会持续给出驱动吗?

3、我看到芯片手册中写道:

 是否因为是关断后电压没有达到正向的0.5V才导致芯片没有进一步开通。