I want to run the IIC usercase on the TDA4VM EVM platform.The source code path is as follows:
pdk_jacinto_08_05_00_36/packages/ti/drv/i2c/example/i2c_utility/i2c_utility_main.c
I use makefile to compile,like this:make -s drv_i2c_utility BOARD=j721e_evm CORE=mcu2_0
and Successfully generated: ti/binary/drv_i2c_utility/bin/j721e_evm/drv_i2c_utility_mcu2_0_release_strip.xer5f
My question is:
1、How will I put this binary file (drv_i2c_utility_mcu2_0_release_strip.xer5f) into the target board (EVM) and running?
2、Where will this print message be displayed,App_consolePrintf(" Board Init FAILED!!!\r\n");
I am using visions_app's SD card to boot(SPL)