从CCS的project中import ccs project功能调入DSPLIB中EXAMPLE的CFFT工程,然后BUILD PROJECT总是出现以下错误:
**** Clean-only build of configuration Debug for project cfft ****
"J:\\program files\\Texas Instrument\\ccsv8\\utils\\bin\\gmake" -k clean
DEL /F "J:\program files\Texas Instrument\c55_dsplib_03.00.00.03\EXAMPLES\CFFT\ccsv5\Debug\cfft.out"
DEL /F "CFFT_T.obj" "TEST.obj"
DEL /F "CFFT_T.d" "TEST.d"
找不到 J:\program files\Texas Instrument\c55_dsplib_03.00.00.03\EXAMPLES\CFFT\ccsv5\Debug\cfft.out
找不到 J:\program files\Texas Instrument\c55_dsplib_03.00.00.03\EXAMPLES\CFFT\ccsv5\Debug\CFFT_T.obj
找不到 J:\program files\Texas Instrument\c55_dsplib_03.00.00.03\EXAMPLES\CFFT\ccsv5\Debug\CFFT_T.d
Finished clean
**** Build Finished ****
Buildfile generation error occurred..
Referenced project 'dsplib' does not exist in the workspace. Project 'cfft' may not build as expected.
Build stopped..
求各位高手帮助。先谢谢了!
郝志强