TPS40060配合单片机做锂电池充电管理,怎么实现对充电过程的管理?输入电压18V或者36V,给12V或者24V锂电池充电,最大电流10A。
我知道要通过单片机采集电池的电压,然后去控制TPS40060的输出电压。现在就是不知道,怎么实现对TPS40060输出的电压进行控制?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢你的回答;BQ24610的最大输入电压为28V,我的设计要求输入至少要达到36V;
TI有能达到36V输入,充电电流最大10A的充电管理IC吗