This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSC1213Y5的一些问题

Other Parts Discussed in Thread: MSC1213Y5

您好,

我现在使用MSC1213Y5(与MSC1210基本相同,只是几个管脚定义不同),其原理图参照TI公司网站提供的参考设计MSC1210EVM设

计原理图,目前单片机可以起振,外部采用有源晶振11.0592M输入,单片机ALE管脚输出4分频2.76482M信号,单片机PSEN管脚也是输出的4分频2.76482M信号。
     现希望加载程序进入FLASH,采用串口烧入的方式(串口烧入需拉高ALE,拉低PSEN),即用TI DOWNLOADER专用串口烧写软件进行烧写程序,其准备工作:
     1)拉低PSEN管脚(打开SW6的5脚),实际测量还是有一个0.9V幅值的4分频2.76482M信号;
     2)拉高单片机ALE管脚(我是外部直接把ALE管脚连到3.3V上);
     3)打开拨码开关SW3中的1.2.3.4.6.7.8.管脚;
     4)最后点击TI DOWNLOADER下载程序,没有反应,弹出一对方框NO reponse to initial CR。
反过来查看单片机是否在工作状态,查看ALE、PSEN管脚是否有输出波形,ALE管脚没有输出波形只是一个3.3V的高电平,另外直接如把PSEN管脚接到地上,还是下载不了程序,感觉只要把ALE、PSEN管脚拉高、拉低,MSC1213好像就没有在工作状态了,ALE上没有波形输出,只是一个高电平。
请帮忙看看可能是什么地方出现问题导致现在的现象。
Best Regards