This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4051: CD74HC4051M96供电电压和High-level input voltage的关系

Part Number: CD74HC4051
Other Parts Discussed in Thread: TMUX1308

您好,CD74HC4051M96目前使用5V供电,针对Channel select S0 S1 S2使用DSP的IO 3.3V电平直接驱动是否可以

如下规格书中是4.5V供电时显示高电平规格是3.15V,5V供电时针对Channel select的高电平没有详细描述。

非常感谢,顺祝国庆中秋快乐。