Part Number: CD74HC4051
Other Parts Discussed in Thread: TMUX1308
您好,CD74HC4051M96目前使用5V供电,针对Channel select S0 S1 S2使用DSP的IO 3.3V电平直接驱动是否可以
如下规格书中是4.5V供电时显示高电平规格是3.15V,5V供电时针对Channel select的高电平没有详细描述。
非常感谢,顺祝国庆中秋快乐。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD74HC4051
Other Parts Discussed in Thread: TMUX1308
您好,CD74HC4051M96目前使用5V供电,针对Channel select S0 S1 S2使用DSP的IO 3.3V电平直接驱动是否可以
如下规格书中是4.5V供电时显示高电平规格是3.15V,5V供电时针对Channel select的高电平没有详细描述。
非常感谢,顺祝国庆中秋快乐。

您好,
下面帖子问题与您的问题一样,答案是:在所有可能的环境条件下,最坏情况下的VIH最高为3.5 V,实际切换阈值在VCC/2附近,但是会有大贯通电流,建议考虑使用TMUX1308。具体请查看下面E2E英文工程师的回复:
CD74HC4051: digital signal logic high threshold VIH for 5V supply