Other Parts Discussed in Thread: AWR1642, AWR1642BOOST
你好!我使用的是AWR1642boost、mmwave-devpack和TSW1400EVM,根据用户手册可以知道利用TSW1400EVM获取的AWR1642的数据是经过奈奎斯特采样后的数字信号,现在我想改变采样的方式(不仅限于改变采样频率等),利用CS的采样方法进行采样,我有以下几点疑问:1、利用TSW1400EVM捕获数据时,可以再RadarStudio软件中调整单个chirp中采样点的个数,例如,默认配置是,采样点256个,采样率10M,也就是单个chirp周期采样25.6us,而射频端ramp时间为60us,我想知道,TSW1400EVM是将完整的周期信号(60us)从AWR1642板中提取出来后,RadarStudio再从TSW1400中截取一段(25.6us);还是说,TSW1400EVM本来就只从AWR1642中获取25.6us的数据;2、利用RadarStudio获取数据时,最开始连接时,BSS FW和MSS FW需要load两个bin文件,这两个文件编译之前的源代码是否有提供,我如果想用CS采样的话是否能从这下手;3、在RadarStudio中设置StaticConfig->Channel Config中设置天线对最后获取的数据包的大小影响不大,与文件SWRA552第8页中提供的数据大小计算方法不符。4、根据AWR1642的设计,两个Tx天线为时分多路复用(TDM),两根Tx天线可以发送不同的chirp信号,使得两根Tx天线能有不同的测量距离和距离分辨率,在RadarStudio中要怎么配置参数才能实现。
谢谢!