我需要设计一款电压跟随器,后端串接47nF电容和发射线圈,线圈接地。我想选一款运放,要求满足6.5V供电电压,单路轨到轨输入,输出,连续输出电流50mA以上,SOC70封装,高负载电容。有没有呀,带宽3M以上,我 没有找见能同时满足要求的呢请大家指点
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据您的电气参数要求,给您选择了两款,LM6584,LM7321. LM7321 有SOIC和SOT23的封装,不知是否可以。 LM6584也是,SOIC或者TSSOP。
如果您需要SC-70的可能没有。
这个有体积要求的,SC-70体积和封装满足替换要求。供电电压6V的有没有呢
LM7321里面的负载电容,我要加入47NF电容,会不会造成失真啊。
LM7321输出电流65mA,LM6584输出75mA,小封装的有没有更高一些的呢。谢谢
您好,我 选用LM7321运放做电压跟随器使用,输出出现了震荡,请参看LM7321输出异常的帖子