按照以下开环电路应用,用按比较器场景应用。工作在25℃。
Datasheet显示失调电压为MAX.7mV (25℃),开环增益为100db,即100000倍。。
失调电压由于有可能V+ > V-和V- > V+两种情况,是不是可以理解为:当INPUT无输入时,OUTPUT在同一批次的运放中,有可能出现0V到VCC-1.5V的任意一个值,可以理解为该应用电路的无INPUT状态是不可控的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM2904 Vos典型值是3mV,远高与0.12mV,所以这样的设计是没法实现比较功能的,失调电压淹没了输入信号。