This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OPA842和OPA836带宽的问题?

Other Parts Discussed in Thread: OPA847, OPA836, OPA842

OPA847跟随衰减电路

要求电路输出阻抗为600,带宽大于40MHz,输出电压范围为5mVp-p~100mVp-p。查阅手册发现OPA847完全满足要求,按手册要求使R3=0,R2=OPEN,Vs=±5V供电。输出接在一个600电阻上(这是要求下一级输入电阻为600,则总负载为1.2K),然后接入RIGOL的100MHz的示波器测量发现带宽只有1MHz左右。最后去掉R4,直接接入50负载电阻到地。发现带宽正常。很好好奇这是为啥?为啥负载电阻大小影响OPA842带宽。如果要实现我的设计要求(输出电阻600,下一级输入电阻600)咋办?这样带宽肯定不够。对了昨天做OPA836问题更大。

OPA836电路也是按照手册上电路做,负载R1之前没有加的。当初要求设计带宽大于10MHz。芯片的频率响应如下:

可见小信号带宽和大信号频率响应是大于10MHz。但问题却来,电路制作完成后测试(输入正弦信号:Vp-p=1V,偏移为2.5V;供电:VS+=5V,VS-=0V)带宽不到100KHz。我没吓了一条,仔细检查电路并未发现问题。查看手册,发现手册测试条件是有一个1K负载,于是加入负载电阻R1=1K。继续测试发现带宽变大,很开心。但发现带宽任然不带到10MHz,大约在2MHz左右。折腾了一个上午后也没有结果。所以发帖,希望大家帮我看看这两个问题。