图片所示,J7接压力传感器,IN+输入信号在3.002v至3.082v之间,IN-输入信号是3.002v,INA333单电源3.3V,放大倍数设置为35倍,Ref电压为1/2*3.3V=1.67V,输出端在IN+在3.022v输入时有输出正常为2.37V,但是IN+端输入再上升大于3.022v后,输出端就上升不了了,维持在2.37V不变了,开始怀疑是共摸输入太大了,但是规格书上了的上限是3.3-0.1V,还是在范围内的,请教下还有什么问题会导致?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
图片所示,J7接压力传感器,IN+输入信号在3.002v至3.082v之间,IN-输入信号是3.002v,INA333单电源3.3V,放大倍数设置为35倍,Ref电压为1/2*3.3V=1.67V,输出端在IN+在3.022v输入时有输出正常为2.37V,但是IN+端输入再上升大于3.022v后,输出端就上升不了了,维持在2.37V不变了,开始怀疑是共摸输入太大了,但是规格书上了的上限是3.3-0.1V,还是在范围内的,请教下还有什么问题会导致?谢谢
您好,应该是输入共模电压超出IC输入范围的问题,我仔细看了数据手册Figure20,其可输入共模电压在输出电压等于供电电源的中间值时最大,随后线性减小。您也可以用我搭的仿真电路测试一下: