求助~~~~!!!!
按照OPA615 datasheet中提供的电路图搭建峰值保持电路,输入64MHz方波(VCXO提供),Vpp=1.5V(0~1.5V),二极管用的是1N4148,电容用50pF,输出电压为1.09V,误差比较大,不知道是什么问题,求大神帮助。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求助~~~~!!!!
按照OPA615 datasheet中提供的电路图搭建峰值保持电路,输入64MHz方波(VCXO提供),Vpp=1.5V(0~1.5V),二极管用的是1N4148,电容用50pF,输出电压为1.09V,误差比较大,不知道是什么问题,求大神帮助。
试试减小电容
如果用的是无极性电容,也可以试试把电容的负端接到一个Vpp/2(=0.75V)的电压上
是二极管1N4148的正向导通电流限制了对电容充放电的速度。
电容I=C*du/dt。
在不考虑二极管导通阻抗及电容ESR的情况下,假设电容恒流充电,则64MHz,1.5Vpp,50pF时,需要的电流为I=C*du/dt=2*C*Vpp*f=2*50p*1.5V*64M=9.6A;
然而1N4148的正向导通电流只有150mA,
可反算,对于50pF的电容,1N4148实际支持的方波频率约为1MHz。