This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何观测逆变器MOS开断对电机相电流的影响?该如何选择放大器?

Other Parts Discussed in Thread: INA240, INA303

MOS开断过程几百ns,想观测这期间的相电流变化情况。这对放大器的带宽提出了什么样的要求?100M够吗?

永磁同步电机,额定电流3.68A,相电阻200毫欧左右。在电机相线上串了5毫欧的采样电阻,那其两端电压在20mV左右,最大50mV左右。母线电压24V,所以放大器的共模输入电压差不多得30V以上吧?共模抑制比CMRR应该得超过10000:1吧?

请问有哪款放大器能够满足上述要求呢?自己找了好久也没有找到,看到一款INA240适用于电机Inline Sensing的信号放大,但是它的带宽只有400KHz,有点低了。

除此之外还有可能存在什么办法可以观测到几百ns内的相电流变化呢?

之前有考虑过用电流探头,但是泰克官网上电流探头的插入阻抗在1MHz的时候最少都得36毫欧,相对于200毫欧的相电阻不可忽略了。并且它随着频率的不同还不一样,这种电流探头应该不合适了吧?

还有考虑过差分探头,但泰克官网上差分探头在1MHz时CMRR只有1000:1左右,也是达不到需求。

还有其他方式吗?