This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运放闭环的相移问题,请大家帮忙看看!!!!

Other Parts Discussed in Thread: OPA277

运放在闭环负反馈应用中,有时候需要评估运放闭环频率响应(包括幅频响应和相位响应),因为这样可以看出运放闭环的带宽和相移.

我们以OPA277运放为例,接成放大倍数Av=3倍的正相输入电路形式,如下图:

OPA277的开环频率响应如下图:

OPA277的SR=0.8V/us,GBP=1M;

第一种情况:

输入小信号,此时闭环的带宽由GBP决定,那么可以通过公式计算出来BW=GBP/Av=1M/3=333k,由带宽可画出闭环的副频响应如下图红色部分:

此时,可近似认为Fc1是闭环传递函数的极点,Fc1对应闭环的相频响应为-45度,这样近似的闭环频率响应就计算出来了。

第二种情况:

输入大信号,闭环的带宽由压摆率和输出波形的Vpp决定,假设输入Vpp=2V,所以输出Vpp=6V,闭环的带宽可以通过公式计算出来:BW=SR/2πVpp=0.8*1000000/(6.28*6)=21.23K,那么问题来了,这个21.23K的频率点是否可以像上面一样,认为是闭环传递函数的极点,同时对应-45度的相移?如果是的话,那闭环下的相移岂不是跟输入信号相关?闭环下的相移到底是由什么决定的?

 

  • 您好,

    我感觉您这里比较乱

    上面附图是运放的开环幅频特性曲线,仅表现的是运放的特性,而您在使用运放时,外加了反馈,下图中的β,即10K、5K反馈网络,那么求闭环频率响应应该由系统的闭环传递函数 VOUT/VIN= Aol/ (1+ Aolβ)绘制出