This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tlvaic3106听不到i2s的声音,请问是不是没有配置好?

Other Parts Discussed in Thread: PCM5102A, TLV320AIC31

你好!在3106的line-out可以听到line-in或者mic-in的声音,但是听不到i2s的声音,i2s的波形测试都正常,如果用一个转换模块pcm5102a(i2s转line-out)通过飞线的方式焊接i2s总线上也可以听到声音,这就说明adv7612输出的i2s是正常的

3106是从模式

请问3106哪里是不是没有配置好?谢谢!

  • 引入的i2s的MCLK=12MHZ,WCLK=48KHZ,BLCK示波器测试有音频数据输入,但是LEFT/RIGHT_LOUT输出端就没有音频数据,请问怎么回事?

    配置的相关寄存器如下:

    tlv320aic31_write(IIC_device_addr[chip_num], 7,  0xa);/* FSref = 48 kHz */ 

    /*left and right DAC power on*/ || soft_reset
    tlv320aic31_write(IIC_device_addr[chip_num], 37, 0xc0);

     /*left DAC not muted*/ 
     tlv320aic31_write(IIC_device_addr[chip_num], 43, 0x0); 

     /*right DAC not muted*/ ~
     tlv320aic31_write(IIC_device_addr[chip_num], 44, 0x0);

    //left-dac
    tlv320aic31_write(IIC_device_addr[chip_num], 82, 0x80);
    tlv320aic31_write(IIC_device_addr[chip_num], 86, 0x08);


    //right-dac
    tlv320aic31_write(IIC_device_addr[chip_num], 92, 0x80);
    tlv320aic31_write(IIC_device_addr[chip_num], 93, 0x08);

    为什么就没有声音?

    如果LINE1或者LINE2接入音频信号,做旁路输出bypss的话,tlv320aic31_write(IIC_device_addr[chip_num], 108, 0xff);  

    LEFT/RIGHT_LOUT有音频输出,芯片外围输出是正常的,

  • 您好,您的意思是如果Line in输入的话,则输出正常,也有声音。
    但如果直接给I2S输入信号, 没有输出是吗?
    那么给的DIN 时序满足要求吗,比如建立时间,保持时间等是否都满足I2S的时序要求呢?
  • i2s时序是没有问题的,现在读取 Page 0 / Register 94: Module Power Status Register发现reg94 = 0xc0,发现 LEFT_LOP/M RIGHT_LOP/M都是powered down,哪里可以设置成powered up?下面是我读取3106的寄存器截图,麻烦看下哪里设置有问题?谢谢!

  • 如果LRCLK和BCLK短碰一下,有时候就有i2s的声音了,很不稳定,请问3106是不是没有识别到时钟信号吗?或者说有 关于3106对于时钟有特殊的配置吗,谢谢!我这里adv7612是主模式产生3个时钟信号和一个数据线,3106作为从模式
  • 您好, 可以看到您的输出部分都已经power down,一个原因是AIC3106 内部有短路保护,一旦发生短路,输出也会disable。 

    另一个看下几个输出的架构,以MONO_LOP/M 输出为例,register 73-78 我看您这边都配置的为0, 也就是line,PGA, DAC都没有routed to MONO_LOP。

    Register 79的MONO_LOP/M也配置的为mute状态呢。

  •  这是我修改的寄存器

     LEFT_LOP/M output driver powered up

    RIGHT_LOP/M is fully powered up

    都已经powered up了,但是i2s就是没有声音,后来把reg2 = 0x00,不分频,line-out就能听到hdmi的声音了,请问是什么原因?