各位工程师您好,我用Bq40z50-R1做电池保护板进行电芯管理。现在测试的过程中发现一个问题。我是7000mAh的电池,等初始参数以及ChemID设定之后,在充电过程中老是出现Remaining Capacity>Full charge Capacity,导致OC置1的现象,而此时的电池电压仅有4.0+或4.1左右,达不到4.2。有时候多经过几个重放的过程,这种现象就没有了。附件有我充电的数据,请帮忙看一下。这种性质不能用于大规模生产的呀,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位工程师您好,我用Bq40z50-R1做电池保护板进行电芯管理。现在测试的过程中发现一个问题。我是7000mAh的电池,等初始参数以及ChemID设定之后,在充电过程中老是出现Remaining Capacity>Full charge Capacity,导致OC置1的现象,而此时的电池电压仅有4.0+或4.1左右,达不到4.2。有时候多经过几个重放的过程,这种现象就没有了。附件有我充电的数据,请帮忙看一下。这种性质不能用于大规模生产的呀,谢谢
找了一上午原因,发现就是RemainingCapacity = FullChargeCapacity触发了OC,然后充电停止了。
进一步分析是,我的Design容量是7000mAh,选择ChemID并且设置了dataMemory里的参数之后 FullChargeCapacity = 6132mAh。这个FullChargeCapacity 就不对。
对于每一个刚加工好的电池组,初始电池电压在3.7(3串),FullChargeCapacity =6132mAh的话,这是不对的呢,这个值能不能修改,还是在一个充放电的循环中,它自己会更新为接近Design的值??
刚刚查了,充电器上的充电电压实际是12.68v,不知道为什么这里的ChargeVol就是12.3V.
你好,能不能加下您的QQ,详细问您一下这个问题。电池要生产了,崩溃中。。。
我的QQ:1548262897
谢谢
补充,知道您说的ChargeVol是12300,是在低温,高温,推荐温度情况下充电电压=12300,在标准温度下ChargeVol=12600. 但是实际的充电器输出电压为12600,二而且实际中,3串的电池最高电压也确实充到了4200.