BQ20Z45的PF状态DFF(DATAFLASH FAILURE)什么条件下会发生?
我们最近一批板,有50%是一上电就会置位DFF,可能是什么原因?
是四串电池。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The only way to recover that is going to be to reprogram the gauge. The most common cause of a DFF is if a DFI file for a different firmware version is programmed on the gauge.
To reprogram the gauge you will need to:
1) Go to ROM mode. Send command 0F00 to command 00 using Pro screen.
2) Program the attached SENC file using the Srec Programming section in the Pro screen.
3) Once programming is finished, send command 08 under the Send SMB Command section of Pro screen.
SLUA404 is a document that will help walk you through configuration, calibration, golden learning, etc.