This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [常见问题解答] BQ76930或bq76940:启动后报告零伏



Q: 为什么用bq76930bq76940启动后某些电池的电压读数为0?

A: bq76930bq76940的电池分为5组,每个电池都有自带电源管脚。

如果上部组未上电,则会在下部组中引起错误,且该组将不会报告电池电压。对于bq76930,上部组中的错误将导致所有电池显示0V。对于bq76940,顶部组中的错误将导致电池6至15显示0V,而电池1至5将显示电压。bq76940中间组上的错误将导致所有电池电压均为0V。

常见检查事项:

  • 确保电池已连接。
  • 确保滤波器组件和IC管脚正确焊接在电路板上。
  • 确保CAP2和CAP3电容器就位且没有短路。
  • 确保已连接TS2和TS3热敏电阻或下拉电阻器已就位。TSn管脚是输入,且必须具有正确参考电压的下拉电阻或热敏电阻才能使器件工作:TS3至VC10X,TS2至VC5X,TS1至VSS。当热敏电阻远程安装且通过连接器连接到系统中时,请确保在电路板测试期间提供替代电阻来模拟热敏电阻。