This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC9881低电压输出异常询问(附上电路图)

Other Parts Discussed in Thread: DAC9881EVM

各位好,

现在使用DAC9881SBRGET再做测试,
电压条件如下
VDD:+5V
IOVDD:3.3V
VrefH-F与VrefH-S:4.096V
VrefL-F与VrefL-S:0V(+5V的GND)
在VrefH-F与VrefH-S间并无使用OPA,是直接标准电压直输,
GAIN:0V
RSTSEL:0V
PDN:0V
LDAC:0V
SDOSEL:3.3V
USB/BTC:3.3V

目前遇到的问题是,
我在CODE设定上面,只要560以下,输出的电压就一直固定在8.9mV
就算CODE设定为0,输出电压依然为8.9mV
但如果CODE大于560以上,那么输出的电压就是依照公式做变化
所以想询问看看,在CODE上面只要560以下电压是否就不会有变化?
或者是我哪边有没有设定好的地方?
恳请各位给予指教,谢谢!!