This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP90080测pTPt1000

Other Parts Discussed in Thread: LMP90080

LMP90080用自带1mA激励源3线法测Pt1000误差比较大,请问是自带激励源的问题吗?
补充:各通道电压校准后比较准,RREF用 1K 1‰ 电阻。请教各位大神

  • 您好,误差有多少?
    理论上来说自带激励源应该是比外接激励更稳定吧。
  • 标准电阻箱                  实测               差值

    842.7                       836.1                -6.6

    1000Ω                      992.3               -7.7       

    1385.1                     1371.8              -13.3    

    1573.3                    1545.7              -27.6

    以上是用标准电阻箱做测试的部分数据
    还有几个问题,我按手册的说明买了-40到150℃的芯片做了耐175℃的电路板,但是在把电路放在不同问下用电阻箱测,差值也是变化的。

    还有个问题是我看到手册上有后台校准,但是没看明白如何使用。不做内置放大处理的话直接打开相关寄存器就可以了吗?还是需要其他配合。

  • 您好,后台校准的流程可直接参考Figure40,后台校准主要针对offset和gain的评估和校正。
    如果不做内置放大,也就是说gain=1,那么后台校准为mode 2,BgcalMode2,那么直接配置BGCALCN=0X2 即可。