This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF80EVM

Other Parts Discussed in Thread: LMK04828, ADC32RF80EVM

TI工程师,

您好 !

ADC32RF80EVM 评估板使用外部时钟时需要将一个信号分为两路同时输入到External Clock Input (J5) 和 LMK04828 Reference Input(J7),这两路信号分别起到什么作用,提供给哪些部件使用?

使用手册上使用2949.12MHz的频率作为外部时钟输入,2949.12MHz是什么频率?使用其他比如1000MHz会与2949.12MHz频率带来哪些方面的差别?如果输入为2949.12MHz的话,意味着此时的最大采样率为2949.12MHz吗?

  • 您好,
    感谢您对TI产品的关注!为更加有效地解决您的问题,我需要多一些时间查看这款芯片,再为您解答。
  • 您好,输入到J5连接器的信号被ADC用作采样时钟。输入到J7的信号是为FPGA(在TSW14J56板上)生成参考时钟,并为ADC和FPGA生成sysref。
    2949.12MHz是采样频率。如数据表所述,最大采样时钟频率为3GHz。

    您可以在下面ADC32RF80EVM页面“设计文件”中,查看原理方块图和原理图:

    https://www.ti.com.cn/tool/cn/ADC32RF80EVM