This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

模拟芯片ADS8698/ADS8688和MCU之间需要完全隔离吗?

Other Parts Discussed in Thread: ADS8694, TIDA-01576, ISO7763

我打算用ADS8694采集模拟量,然后通过SPI通讯到MCU,但是不知道是否需要和MCU之间完全隔离,用隔离DCDC,SPI用ISO7763隔离?还是电源不需要隔离,GND接在一起,但是这样的话我觉的SPI隔离也不是很有必要了,反正gnd是相通的,spi直接连就行了,我看了TI的几个测试板原理图,TIDA-01576系列,由于测试板没有包括mcu,所以不知道是否需要和muc完全隔离,但是这几块测试板除了一块,spi通讯都用了iso芯片隔离,请问完全隔离和单单spi隔离,对采集精度上有区别吗?如果电源不隔离,这个spi隔离是否需要?还是只要adc电源芯片和mcu的电源芯片但凡不是同一个,就需要spi隔离?

  • 您好,
    隔离一般是为了隔离高压或噪声,如果仅对信号进行隔离,电源不隔离确认没有隔离的意义;是否对采集精度有影响,需要看隔离前后供电电源的性能和是否对采集信号有影响