This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274工作时序问题

Other Parts Discussed in Thread: TMS320F2808, ADS1274, ADS1232

看了ADS1274的官方文件,但是没怎么懂。我用TMS320F2808来驱动,电路图如图,按照我的这种连接方式,将DSP设置为主机模式,

采用虚发数据的方式读取数据,每次发送8位,相应的能读取到8位数据,连续3次就可以读取到24位,

CLK:25MHZ

读取数据时将SYNC置为低电平,延时10ms然后开始读取数据,读取完毕后再置为高电平。

但是我读取出来的数据一直为0,输入端的电压有1.1V,用示波器查看几个引脚的信号,都有波形出来,MISO端出来的是一个标准的方波。

现在不知道问题出在哪里。还是我的驱动方式有问题,请专家帮忙!

x 出现错误。请重试或与管理员联系。