使用8148接GV7600输出SDI信号,然后通过lmh0307一分二。现在一分二后接到显示器SDI信号很不稳定,总是出现黑屏,看起像是信号中断一下。
如果直接用GV7600输出的SDI信号给到显示器,则没有这个现象。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用8148接GV7600输出SDI信号,然后通过lmh0307一分二。现在一分二后接到显示器SDI信号很不稳定,总是出现黑屏,看起像是信号中断一下。
如果直接用GV7600输出的SDI信号给到显示器,则没有这个现象。
有电路图吗? 输出Enable是否已经拉高?另外,黑屏的话,LMH0307的FAULT输出引脚什么状态?
hi Kailyn Chen,
SDI电路见附件。
我们LMH0307没做任何配置,黑屏时没有测量过FAULT输出状态。不是一直黑屏,是黑一下,马上有好了。
hi Kailyn Chen,
SDI电路见附件。
我们LMH0307没做任何配置,黑屏时没有测量过FAULT输出状态。不是一直黑屏,是黑一下,马上有好了。
看电路没什么问题,黑屏马上又好,像是不稳定。
最好是监测黑屏时fault的输出状态,或者读一下状态寄存器0x01h的情况看是否有哪里报错。
就是不稳定,因为黑屏就是闪一下,所以很难在黑屏时读取寄存器状态。 我们随机读取0x01h寄存器,有两种值:0x1B,和0x12。
0X12和0X1B这两种,bit1和bit3都为1,问题在SDI0,SDI1上报错。可以先不接显示屏,用示波器测量下LMH0307的SDOUT的输出是否一直有信号。