我使用DS90UB914A 和 DS90UB913A连接一个CMOS,913和914只设置了和IIC相关的寄存器,目前可以通过914设置远端的913和CMOS,CMOS初始化正常,输出的波形也都没有问题,但是914这一端输出的PCLK是913输入端的2倍,但是输出的VS是对的,都是30帧,请问这个是什么问题,非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
913 您是采用外部晶振提供的时钟把,然后采用的是10bit mode是吗?
在datasheet 8.4.1部分有介绍,可以看到,10 bit mode,pixel clock和外部晶振的比值是2, 12bit的话,比值为1.5.
换句话说,10bit mode,如果913外部晶振提供48MHz的时钟的话,那么PCLK的时钟需要96MHz。
这应该是您指的914输出PCLK是913输入时钟的2倍关系的原因。 具体可参考datasheet中的描述。