我们在使用TXS0108E的时候,用它来做1.8V到2.8V的电平转换,后级接了4路信号,3路用于电源芯片的EN控制,一路用于一个工作在开关状态的三极管,结果发现2.8V输出端的电平会被拉到0.9V。通常情况下,我们用于使能控制和三极管导通截止都不需要太大的电流,而手册中的最大驱动电流应该是+/-50mA才对,为什么会造成这种现象?是否有P2P的可推荐的产品来解决这个问题,我们板子已经贴好了,在调试过程中发现的这个问题。非常感谢各位的帮助!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们在使用TXS0108E的时候,用它来做1.8V到2.8V的电平转换,后级接了4路信号,3路用于电源芯片的EN控制,一路用于一个工作在开关状态的三极管,结果发现2.8V输出端的电平会被拉到0.9V。通常情况下,我们用于使能控制和三极管导通截止都不需要太大的电流,而手册中的最大驱动电流应该是+/-50mA才对,为什么会造成这种现象?是否有P2P的可推荐的产品来解决这个问题,我们板子已经贴好了,在调试过程中发现的这个问题。非常感谢各位的帮助!
TXSxx系列和TXBxx系列的电平转换芯片输出驱动能力很小,达不到+-50mA的驱动。 驱动能力参考Ioh,Iol电流大小。
您需要多大电流输出? 带方向控制位的SN74系列的电平转换驱动能力比较高,能达到+-32mA。比如8bit的SN74LVC8T245.