你好,有如下几个问题烦请帮忙解答下,谢谢。
1:想要做一款DP(DP1.2&DP1.4 DP++) to HDMI(4KX2K@60Hz)的产品,是否可用SN65DP159?datasheet上写的只支持DP1.1,如果它只支持DP1.1,带宽是达不到4KX2K&60Hz的。
2:49pin较40pin多了哪几项功能,datasheet上没看清区别。
3:此颗芯片是否有HDMI在4KX2K@60Hz的闪屏问题。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,有如下几个问题烦请帮忙解答下,谢谢。
1:想要做一款DP(DP1.2&DP1.4 DP++) to HDMI(4KX2K@60Hz)的产品,是否可用SN65DP159?datasheet上写的只支持DP1.1,如果它只支持DP1.1,带宽是达不到4KX2K&60Hz的。
2:49pin较40pin多了哪几项功能,datasheet上没看清区别。
3:此颗芯片是否有HDMI在4KX2K@60Hz的闪屏问题。
谢谢。
1. 不支持DP1.4, 只能支持到DP1.1的标准。这里 6Gbps 的data rate指的是HDMI 2.0,不是DP standard,The SNx5DP159 device supports data rate up to 6-Gbps per data lane to support Ultra HD (4K × 2K / 60-Hz) 8-bits per color high-resolution video。
2. 您这里应该指的40Pin的RGZ和40Pin的RSB封装,多的8pin 可以在Pin Functions 中对比看到,比如48pin的多了AUX_SRCp,AUX_SRCn等引脚。
3. 数据手册中是能支持到4KX2K@60Hz分辨率,这个也是经过试验得到的结论,合理的设计以及layout,显示是没有问题的。