This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我手头有块板卡,是用DP83867E 与另一个chip(ksz9477)的sgmii mac接口通过四线方式连接,也就是SGMII in、out两对差分 且AC耦合方式连接,并且对LED0、LED1、RX-CTRL配置为mode2、mode4和mode3,在power up过程中,可以用示波器看到电压依次是0.45v,1.91v和0.63v,满足模式要求的电压。
另外我检查了时钟,是1.8v 25M,用差分线头测试SGMII-SIP和SIN有信号,而SGMII-SOUTP\SOUTN没有差分信号,MDI四对差分线也没有信号。正常应该是可以看到载波。
用网线连接PC,PC显示也是个红叉。
我正准备买个msp430 launch pad 对寄存器进行操作,估计得几天后的事情了。
请熟悉的专家给出出招。