根据这个参考设计做的,无论怎么调节C2、C3、C4,R2效果都不大,
现在C2是0.022uF,C4改成了RC,R是2.2K,C是0.022uF,R2是910Ω,R8用的1K,D7是4.3V,其他参数和参考设计一样
现有以下问题:
LED功率从较小调到2/3功率时,MOS管Q1都比较烫,Q1和调光效果是个矛盾体,增大R8,MOS管发热减小,调光效果变差,反之亦然
功率小于4W时有轻微抖动
70%总功率调光时,有一个0.6W左右的突变
希望哪位给指点下,在此谢过
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.