This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【DIY】 LM3447应用

Other Parts Discussed in Thread: LM3447

用于使用 LM3447应用

85-265Vac输入,输出25Vmax,恒流600mA

设计的主要目的在于:

展示 LM3447 是使用单级 PFC、隔离式 LED 灯驱动器实现高可调光性能的理想选择,同时具有简单、组件数量少和解决方案尺寸小等优势。

 

●85VAC 至 264VAC、50Hz 输入电压

●15V 至 25V LED 电压

●300mA LED 调节电流

●>85% 典型的系统效率 ●高功率因数 > 0.9 ●输出短路和开路保护