请问TAS2563可以在PPC3软件中设置96kHz采样率么?

Other Parts Discussed in Thread: TAS2559, TAS2563

我们使用过TAS2559数字功放。虽然在芯片手册上说明可以配置为采样率8k~96kHz,但是当我们使用为ROM模式时,在PPC3软件上只能找到16kHz和48kHz两个选项。现在由于I2S总线时钟是共用的,为了兼容其他设备,我们需要将功放的采样率设置为96kHz或192kHz,请问更换TAS2563芯片能解决这个问题么?TAS2563芯片工作在ROM模式时可以在PPC3软件上配置为96kHz或者192kHz么?

  • 您好,TAS2550在使用ROM mode时,采样率能达到96Khz,但是当speaker protection system在运行的时候,采样率只能达到48KHz。
    所以您看下PPC3的设置中,是否将speaker protection disable掉导致不能设置96KHz。
  • 非常感谢。我们查找了PPC3,“home”页共有“System Checks”、“Characterization”、“Tuning and Audio Processing”、“Device Control”、“Direct I2C”、“Test and Measurement”和“End System Integration”几个页面,我们找不到可以将speaker protection disable的地方,请问在哪个页面下设置?